VBUS.UVWTHRESH

Description

This parameter is the DC bus undervoltage warning threshold. When the measured DC bus voltage falls below the threshold, an undervoltage fault is thrown for each axis.

Examples

Usage

The drive configures the default value for this parameter based on power electronics ratings.

When the measured DC bus voltage VBUS.VALUE is less than VBUS.UVWTHRESH, the drive reports Warning 2007: Bus under voltage (See W2007). When VBUS.VALUE is greater than VBUS.UVWTHRESH, the warning is removed.

Code

The following example demonstrates the DC bus undervoltage warning check. When the bus voltage is greater than the warning threshold, the undervoltage warning is not reported.

--> VBUS.UVWTHRESH 100
--> VBUS.UVWTHRESH
100 [Vdc]
--> VBUS.VALUE
162.297 [Vdc]
--> DRV.WARNINGS

No warnings active

When VBUS.VALUE is less than VBUS.UVWTHRESH, the warning is reported on each axis.

--> VBUS.VALUE
96.895 [Vdc]
--> DRV.WARNINGS
1-2007: Warning: Bus under voltage.
2-2007: Warning: Bus under voltage.

Context

For more information on DC bus voltage protection, refer to Power View and Regeneration.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units VDC
Range 0 to 900 VDC
Default Value Dependent on drive model
Data Type Integer
See also VBUS.UVMODE, VBUS.UVTHRESH, VBUS.VALUE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

VBUS.UVWTHRESH

300ah

03h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2511

1

2511 (0x9cf)

VBUS.UVWTHRESH

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.UVWTHRESH

2511

Unsigned16

Read/Write

-